Carrier Setup Continuous Wave
1. General Settings
Enabled
Choices: On | Off
Default: On
Enable or disable the carrier in waveform generation.
Displays the state of the carrier in waveform generation.
Frequency Offset
Range: -4GHz to 4GHz
Default: 0
Set the frequency offset to the carrier signal in Hz.
Power Boosting
Range: -40 to 40dB
Default: 0dB
Set the power boosting of the carrier relative to others.
Initial Phase
Range: 0 to 360
Default: 0
Enter the initial phase of the carrier signal in degrees.
Carrier Type
Choices: Downlink | Uplink | PRACH | ContinuousWave
Default: Downlink
Select the carrier type.